AXIS#.FAULTS

Description

Indicates what faults are present on an axis.

Examples

In a scenario where two faults are present on Axis 1 (faults 4312 and 4115), the following output would be seen:

-->AXIS1.FAULTS

4312: Feedback: Broken Wire fault.

4115: Failed to set feedback type.

Versions

Action Version Notes
Implemented 02-00-00-000  

General Information

Type Read Only
Units N/A
Range N/A
Default Value N/A
Data Type String
See Also DRV.FAULTS

Stored in Non Volatile Memory

No

Variants Supported

Supported on all device types.